cancel
Showing results for 
Search instead for 
Did you mean: 

Timer enable blocks rest of main function.

estersci2
Associate III
Posted on September 24, 2015 at 18:17

I am new to timers. If anyone can see a fundamental mistake, please advise.

I have set up a time interrupt callback function which simply increments a integer. 

It is based on a LED blinking example, so shouldn't saturate the processor?

Anyway, I have found that when I call the time and interrupt enable in my main function, not one single line after that point in my main function gets executed. 

Is this normal?

int main(void)

{

  SC_State SCState = SC_POWER_OFF;

RCC_Configuration();

 

  NVIC_Configuration();

 

  TIM3_Configuration();

    

  TIM3_Enable();

flag++;  // this never increments

// nothing that follows ever gets executed

.......

and the rest of my functions below.....

void RCC_Configuration(void)

{

  /* --------------------------- System Clocks Configuration -----------------*/

  /* TIM3 clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

 

  /* GPIOD clock enable */

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

}

 

/**************************************************************************************/

 

 

/**************************************************************************************/

 

void NVIC_Configuration(void)

{

  NVIC_InitTypeDef NVIC_InitStructure;

 

  NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

}

 

/**************************************************************************************/

 

void TIM3_IRQHandler(void)

{

  if (TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET)

  {

   testing++;

  return; //also tried it without this return

}

}

 

/**************************************************************************************/

 

void TIM3_Configuration(void)

{

  TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

  uint16_t Period, Prescaler;

 

  Prescaler = 10000;

  Period = ((SystemCoreClock / (2 * Prescaler)) / 4); // Period for 4 Hz frequency

 

  /* Time base configuration */

  TIM_TimeBaseStructure.TIM_Prescaler = Prescaler - 1;

  TIM_TimeBaseStructure.TIM_Period = Period - 1;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);

 

  /* TIM3 enable counter */

  

}

void TIM3_Enable(void)

{

TIM_Cmd(TIM3, ENABLE);

 

  TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE);

}

void TIM3_Disable(void)

{

TIM_ITConfig(TIM3, TIM_IT_Update, DISABLE);

TIM_Cmd(TIM3, DISABLE);

   

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Chris1
Senior III
Posted on September 24, 2015 at 22:46

You need to clear the appropriate interrupt flag(s) in your IRQ handler, unless you want to keep executing that function forever...