Timer: clearing update event flag can cause flagless input capture interrupt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-22 11:31 AM
.ExternalClass8CE9ECEBE1E84036AC5D7158FC9B07F8 p {margin-bottom:0.08in;}
The goal is to measure durations between input captures that exceed the 16 bit counter range by adding counter overflows. There appears to be no way to cleanly do this. The basic problem is that clearing the update-event interrupt flag is a read-modify register-write type of operation. During that short window a signal that causes an input capture will turn on the input capture flag, and then have it immediately reset by the write operation that is clearing the update-event flag. The result is that an input capture interrupt follows, but there will be no flag set.
This situation is rare, but I have caught instances of it happening. In my particular case I am able to treat an input capture interrupt with no flag set the same as if the flag were set and the results are correct, however in the general case this would not work when more that one input capture in a timer was being used as the routine would not be able to tell which channel was the cause of the flagless interrupt. Is the some way around this problem? Might DMA avoid the problem, (if the DMA channels are not tied up!)? #input-capture #timer- Labels:
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-22 1:25 PM
Why not use the prescalar - or cascade 2 timers to form a 32-bit timer?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-22 5:25 PM
One potential issue with M3 designs is a pipeline hazard with the peripheral vs NVIC. If you clear the interrupt as the last thing before exiting an interrupt handler the pipelining, write buffers and disparity in clocks will create a condition where the peripheral is still signalling the interrupt when the M3 decides to tail-chain, causing the handler to reenter (priorities may impact which) and the peripheral will have cleared when you look at it. To avoid this be sure to clear the interrupt upon entry. ie Check source, dismiss, process, leave
As to your issue about knowing which epoch of the 16-bit timer you're looking at. Take a look at using the core cycle counter for a long term timebase, the 32-bit counter has an epoch >1min. The cycle counter is part of the trace unit, and is present in all STM32 parts I've checked.https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DispForm.aspx?ID=15729&RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/frequency capture&Source=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder%3D%252Fpublic%252FSTe2ecommunities%252Fmcu%252FLists%252Fcortex%255Fmx%255Fstm32%252Ffrequency%2520capture%26FolderCTID%3D0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5
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
‎2011-10-22 6:11 PM
Even following Clive's advice, it is still possible to lose an interrupt as Don has discovered. In my case, it was impossible for the frequency to change beyond certain bounds between samples, so I performed a logic test to determine when an interrupt was lost, and adjusted for it.
I previously coded the same application for the Texas Instruments MSP430 running at 8 MHz, and never had the problem. The STM32 is still a better choice, but I wish that ST would find a hardware fix for this. Cheers, Hal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-22 6:44 PM
I can't say I've observed it lose interrupts in this fashion, if you push the frequency too high you will saturate the processor.
A better method might be to use encoder/counter mode and periodically sample it, and time stamp using the core counter. Then infer frequency from that. Personally I find these 16-bit timers/counters to be a total cop-out in a 32-bit design. There are so much better ways to build A-B timers, frequency generators and prescalers.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-23 9:55 AM
Clive1: thanks for the thoughts--
The highest possible resolution is required so getting longer times via the prescalar is not an option. Using two counters in cascade would be a possible solution, and one I had not thought of. Having 32 bits takes care of the case where the input captures are one second apart. If the time intervals would happen to be much longer the problem would arise again. Basically, it is a mistake in the hardware design. There needs to be a register where writing a ''1'' clears the flag, not writing a ''0''. Motorola/Freescale has always done it this way. When we realized what was going on, a friend that has many decades of experience made the comment, in jest, that the hardware designer should be dragged out and flogged. .- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-23 11:24 AM
Every manufacturer's products has pros and cons. Perhaps you may want to look at the NXP LC17xx which has four (4) 32-bit timers with 32-bit prescalers.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-23 12:37 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-23 12:52 PM
As I said, no matter who you go with, you will find issues. For Cortex-M0/3/4 parts, I currently use FreeScale Kinetis, NXP LPC1xxx and STM32F parts. Fortunately for me, my development tool chain supports all 3 device families (and several others as well, such as Atmel, Energy Micro, Stellaris, Nuvoton, etc., should the need arise).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-10-23 2:07 PM