2013-05-28 1:49 PM
I'm just stering with the STM324f Discovery board and am trying to get timer 5 setup as a free running 1us timer that I can access in my code for timing. No matter what I do, I can't get TIM5->CNT to change from zero. Any idea what I'm doing wrong? Here's the relevent code in main():
/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */
#define
PLL_M 8
#define
PLL_N 336
/* SYSCLK = PLL_VCO / PLL_P */
#define
PLL_P 2
/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */
#define
PLL_Q 7
int
main()
{ SystemInit(); TIM5->CR1
= 0;
// disable timer 5
TIM5->
DIER
= 0;
// no interrupts
TIM5->
CNT
= 0;
// reset timer value
TIM5->
PSC
= (PLL_N / PLL_P) - 1;
//
prescaler
TIM5->
ARR
= 0xFFFFFFFF;
// reload value
TIM5->
EGR
= 1;
TIM5->CR1
= TIM_CR1_CEN;
// enable timer 5
RCC->
APB1ENR
|= RCC_APB1ENR_TIM5EN;
TIM5->SR
= 0;
// reset flags2013-05-28 2:12 PM
First rule of synchronous logic, have a clock.
Turn ON the clock first, otherwise the register writes won't work.RCC->
APB1ENR
|= RCC_APB1ENR_TIM5EN;