cancel
Showing results for 
Search instead for 
Did you mean: 

TIM5 timer problem

elis
Associate
Posted on June 10, 2012 at 16:47

There is a missing table in RM0090

para: 14.4.3 TIMx slave mode control register (TIMx_SMCR),

Table 60: TIMx internal trigger connection on page 395

I am trying to use TIM1 timer as a prescaler to TIM2 and TIM5 timers and this table is supposed to specify the ITRx signals routing for these timers. But, there is no table.

If you look to the rest of the page, there are missing bit descriptions too.

Eli
3 REPLIES 3
Posted on June 10, 2012 at 17:07

Definitely missing.

The STM32F2 reference might be instructive as they share a very common peripheral set. Page 398 & 399

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/REFERENCE_MANUAL/CD00225773.pdf

The actual function should be easy enough to validate.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
elis
Associate
Posted on June 11, 2012 at 14:21

Thank you for your advice. I used TIM8 instead of TIM1 (according to the table that you referred) and it worked like charm.

Eli.

vitaliy2
Associate
Posted on July 11, 2012 at 16:54

See also table 62 on page 437 in RM0090.