2009-07-27 10:47 PM
TIM3 BIE int. problem
2011-05-17 4:18 AM
Hi
I'm using STM32 ACIM library v 2.0 on STM32F103ZET6 MPU If I run program normal it hang. So I use debugger and see that BIE flag in timmer1 is on. If I remove this flag, program run. Im using KEIL uVision3 Well I have also some other problem (give me over current error) I use trimer on PC1 and PC2 but stil got error. I'm new on ST MPUs Until now I use NXP ARM7. best regards Simon2011-05-17 4:18 AM
My mistake :(
Problem was, becouse I don't connect PE15 pin. Only I don't understand why hand up and display not start. Since to be bug....