cancel
Showing results for 
Search instead for 
Did you mean: 

TIM2 Input capture prescaler

michaellange9
Associate II
Posted on January 30, 2009 at 09:45

TIM2 Input capture prescaler

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
michaellange9
Associate II
Posted on May 17, 2011 at 13:01

Hello,

I measure the time between two rising signal edges with TIM2. To get the best resolution I'm trying to change the timer prescaler on the fly. Means that when the captured value is to small I will reduce the prescaler.

But this is not working. I can change the prescaler but the values in the CCR1 does not change. When I choose a smaler prescaler in the initialisation routine in the beginning, it's ok.

It seems that the preloades prescaler value is not overtaken. But when I read back the value the new one is there.

Any ideas what is going wrong?

Michael

Here is the code:

vu16 time_6steps;

void TIM2_Configuration(void)

{

/* Clear the IT pending Bits */

ClrBit(TIM2->SR,TIM_SR_UIF);

ClrBit(TIM2->SR,TIM_SR_TIF);

ClrBit(TIM2->SR,TIM_SR_CC1IF);

ClrBit(TIM2->SR,TIM_SR_CC2IF);

/* ----- Time Base Configuration ----- */

TIM2->PSC = 2000;

//TIM2->ARR = U16_MAX; //???necessary

TIM2->RCR = 0; //Delete repitition counter register

/* ----- Timer Mode Configuration -----*/

ClrBit(TIM2->CR2,TIM_SMCR_SMS); //Reset Mode

ClrBit(TIM2->CR2,TIM_SMCR_SMS+1);

ClrBit(TIM2->CR2,TIM_SMCR_SMS+2);

SetBit(TIM2->CR2,TIM_CR2_TI1S); //Channel inputs are XOred

SetBit(TIM2->SMCR,TIM_SMCR_TS);

ClrBit(TIM2->SMCR,TIM_SMCR_TS+1);

SetBit(TIM2->SMCR,TIM_SMCR_TS+2); //Filtered Timer Input 1 (TI1FP1)

ClrBit(TIM2->CR1,TIM_CR1_DIR); //Counter Mode upcounting

ClrBit(TIM2->CR1,TIM_CR1_CMS); //Counter Mode edge aligned

ClrBit(TIM2->CR1,TIM_CR1_CMS+1); //Counter Mode edge aligned

ClrBit(TIM2->CR1,TIM_CR1_OPM); //Counter Mode one pulse disable

ClrBit(TIM2->CR1,TIM_CR1_ARPE); //Counter Mode auto reload preload register disable (ARR not bufferd)

/* ----- Channel Configuration ----- */

/* --- Channel 1 --- */

//Input capture

ClrBit(TIM2->CCER,TIM_CCER_CC1P); //Trigger at rising edge

SetBit(TIM2->CCMR1,TIM_CCMR1_CC1S); //Triggerinput is TI1

ClrBit(TIM2->CCMR1,TIM_CCMR1_CC1S+1);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC1F);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC1F+1); //Input Filter

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC1F+2);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC1F+3);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC1PSC); //Input prescaler

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC1PSC+1);

SetBit(TIM2->CCER,TIM_CCER_CC1E); //Enable Capture CH1

/* --- Channel 2 --- */

//Input capture

SetBit(TIM2->CCER,TIM_CCER_CC2P); //Trigger at falling edge

ClrBit(TIM2->CCMR1,TIM_CCMR1_CC2S); //Triggerinput is TI1

SetBit(TIM2->CCMR1,TIM_CCMR1_CC2S+1);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC2F);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC2F+1); //Input Filter

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC2F+2);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC2F+3);

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC2PSC); //Input prescaler

ClrBit(TIM2->CCMR1,TIM_CCMR1_IC2PSC+1);

SetBit(TIM2->CCER,TIM_CCER_CC2E); //Enable Capture CH2

/* --- Channel 3 --- */

//Output compare mode

ClrBit(TIM2->CCMR2,4); //Output compare mode frozen, no effect of comparisions

ClrBit(TIM2->CCMR2,5); //Register CCMR3, Bits OC1M 0-2

ClrBit(TIM2->CCMR2,6);

/* ----- Interrupt source -----*/

//SetBit(TIM2->DIER,TIM_DIER_UIE); //Enable update Interrupt

//SetBit(TIM2->DIER,TIM_DIER_TIE); //Enable trigger Interrupt

SetBit(TIM2->DIER,TIM_DIER_CC1IE); //Enable capture CH1 Interrupt

SetBit(TIM2->DIER,TIM_DIER_CC2IE); //Enable capture CH2 Interrupt

//SetBit(TIM2->DIER,TIM_DIER_CC3IE); //Enable capture CH3 Interrupt

}

###############################################

void adjust_prescaler(void)

{

if(time_6steps

{

TIM2->PSC = 100; //new prescaler

}

}

#############################################

void TIM2_IRQHandler(void)

{

if(CheckBit(TIM2->SR,TIM_SR_CC1IF)) //rising edge?

{

time_6steps = TIM2->CCR1;

TIM2->CNT=0; //clear Counter

}

ClrBit(TIM2->SR,TIM_SR_CC1IF);

ClrBit(TIM2->SR,TIM_SR_CC2IF);

/* Generate TIM1 COM event by software */

SetBit(TIM1->EGR,TIM_EGR_COMG);

}