cancel
Showing results for 
Search instead for 
Did you mean: 

TIM1: can I change Dead Time on the fly ?

JMED.1
Associate

I need to change the dead time of the TIM1 complementary outputs cycle by cycle. What is the behavior if I just overwrite the DTG[7:0] value during a cycle: does it change the actual dead time of the next cycle? or the current?

Thank you in advance.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Uwe Bonnes
Principal III

As long as no locking is set, the reference manual implies that you can change the DTR value.and that should have an effect!