2019-04-30 3:53 AM
Hello,
when generating a STM32CubeMX project from within Keil µVision, in stm32f4xx_hal_tim.c (STM32F4xx_DFP/2.13.0) the function TIM_ETR_SetConfig is defined as static in the .c file and none-static in the corresponding .h file, so i need to change this manually to make the project compile. Is this a Bug in STM32CubeMX or has it to do with Keil µVision?
C:/Keil_v5/ARM/PACK/Keil/STM32F4xx_DFP/2.13.0/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_tim.c(161): error: static declaration of 'TIM_ETR_SetConfig' follows non-static declaration
static void TIM_ETR_SetConfig(TIM_TypeDef* TIMx, uint32_t TIM_ExtTRGPrescaler,
^
./RTE/Device/STM32F429IITx/STCubeGenerated/Drivers/STM32F4xx_HAL_Driver/Inc\stm32f4xx_hal_tim.h(1938): note: previous declaration is here
void TIM_ETR_SetConfig(TIM_TypeDef *TIMx, uint32_t TIM_ExtTRGPrescaler,
^
C:/Keil_v5/ARM/PACK/Keil/STM32F4xx_DFP/2.13.0/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_tim.c(5368): error: static declaration of 'TIM_ETR_SetConfig' follows non-static declaration
static void TIM_ETR_SetConfig(TIM_TypeDef* TIMx, uint32_t TIM_ExtTRGPrescaler,
^
./RTE/Device/STM32F429IITx/STCubeGenerated/Drivers/STM32F4xx_HAL_Driver/Inc\stm32f4xx_hal_tim.h(1938): note: previous declaration is here
void TIM_ETR_SetConfig(TIM_TypeDef *TIMx, uint32_t TIM_ExtTRGPrescaler,Best Regards
Thomas