2017-09-27 2:17 AM
Dear all,
What are the wakeup pins of the STM32F413VGT? CubeMX and the reference manual says three (PA0/PC0/PC1) but the generated code won't accept PC0 and PC1. And when I write directly into the PWR_CSR register for the two pins, PA0 stops waking up the MCU out of standby. I'm a little bit confused, have I missed an imported part?
Kind regards,
Age
Solved! Go to Solution.
2017-09-27 5:55 PM
Solved it! The answer is, there are three wake up pins PC0, PC1 and PA1 you can use.
2017-09-27 5:55 PM
Solved it! The answer is, there are three wake up pins PC0, PC1 and PA1 you can use.