cancel
Showing results for 
Search instead for 
Did you mean: 

The solution for a 800×480 LCD based on STM32

albhuang
Associate II
Posted on March 07, 2014 at 10:40

Hi everyone,

   I'd like to choise STM32 for a HMI case, whoes main requirement was a TFT LCD of 800*480. There were 2 idea:

1) STM32F1 + RA7785

2) STM32F429

Which was the better? Everybody could give me some suggestion.

By the way, STM32F429VG(LQFP100) had LCD interface?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 07, 2014 at 13:33

Hi Albert,

STM32F429VG features an LCD parallel interface and an LCD-TFT controller with a dedicated Chrom-ART Accelerator.

More details on this product

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1577/LN1806/PF255430

.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.