Skip to main content
Associate II
September 2, 2024
Question

The puzzled about SWPMI of STM32H7

Hi Sir ,

    I need your help with some questions about SPWMI:

1. STM32Cube_FW_H7_V1.7.0 without Demo project, Could you provide a Demo project of SWPMI STM32H7?

2. As RM said,SWPMI can serve only as Master interface, Whether SWPMI can communicate with itself ? such as Board1 SWPMI (transfer)  communicate  with Board2 SWPMI (receiver) . 

3.When internal transceiver is bypassed(SWP_TBYP=1),the SWPMI_TX、SWPMI_RX and SWPMI_SUSPEND signals can connect an external transceiver. I don't find the profile about external transceiver.Could you please prodive the specific device or profile of external transceiver?

    Looking forward to your reply!

 

This topic has been closed for replies.

2 replies

Lead II
September 5, 2024

As I understand: SPWMI is just a master on STM32 MCU.
It does not have a slave receiver (or mode).

So, it cannot communicate with itself.

You might be able to test it with these single wire LED strips.

SONGTAOSIAuthor
Associate II
September 5, 2024

Thank you for your reply.

I have tested it and  really cannot communicate with itself.

Now, I want bypass  internal transceiver, and use SWPMI_TX、SWPMI_RX and SWPMI_SUSPEND signals  connect an external transceiver, I don't find the device which satisfy ETSI TS 102 613 tcchnical in st.com .Could you please prodive the specific device(part number)  of external transceiver?