2013-11-11 2:07 AM
we are trying to make a communication between the Mc and the Accelerometer
I see that the clock and data don't work right as on the scope I see the data and clock transitions are making together in the same time while the data must be settled before the rise edge of the clock attached image from the scope to the signal also I tried to make I22 using bit banging but the rise time and fall time of the port is 20Micro second which is exceed the max rise and fall time how to make this time less than 300 nano second2013-11-12 8:29 AM
The attached image looks ok to me but there is no acknowledge from the slave.
Maybe you use wrong address or maybe the slave doesn't support write operation.