cancel
Showing results for 
Search instead for 
Did you mean: 

The external RTC clock of stm32f765igt6 chip,the waveform of the clock is very small,RTC clock is very inaccurate.This is whether the crystal oscillator or capacitor selection problem, or our single-chip RTC drive problem;

晓杨.1
Associate

For the external RTC clock of stm32f765igt6 chip, we use a 32.768KHz crystal oscillator of Epson, which is equipped with 10PF capacitor. Some of them will make the MCU unable to start, and reduce the capacitance value to 2pF, MCU can start, but we actually measured the waveform of the clock, and found that no matter what kind of configuration, the amplitude of the signal is very small, basically can not see the signal; at the same time, there is a problem to change the board with 2pF capacitor, RTC clock is very inaccurate, one night time, it will be 10 minutes;

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The application note AN2867 contains a lot of hints on the use of crystal oscillators. Escpacially section 4.1 (Low-speed oscillators embedded in STM32 microcontrollers) and section 7 (Tips for improving oscillator stability) might be very helpful for you. It is not a good idea to measure the amplitude of the LSE directly at the crystal pins, because even the load of the probe is too high. You could route the LSE internally to the pin MCO to measure the frequency.

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.