cancel
Showing results for 
Search instead for 
Did you mean: 

Temperature measurement

IK.1
Associate II

I read TS_CAL1 and TS_CAL2 values from stm32f303vc and saw that TS_CAL2 is lower then TS_CAL1. Is it correct? I think this is mistake. I check the memory with Visual Studio in debug mode and saw the same values. Why is it so?

Thank u in advance!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
IK.1
Associate II

Datasheet shows the following addresses:

1) for TS_CAL1 0x1FFF F7B8 - 0x1FFF F7B9

2) for TS_CAL2 0x1FFF F7C2 - 0x1FFF F7C3

Are they correct?

IK.1
Associate II

I think now that was correct. I checked my current temperaute adc values and saw that they are approximately equal to TS_CAL1. it seems to me that values are high with low temperature and low with high temperature. May be it will be useful for someone.