2010-05-04 8:24 AM
SysTick.CTRL register documentation
2011-05-17 4:49 AM
From RM0008 STM32 Reference Manual (13902.pdf)
Pg 71 ''The RCC feeds the Cortex System Timer (SysTick) external clock with the AHB clock divided by 8. The SysTick can work either with this clock or with the Cortex clock (AHB), configurable in the SysTick Control and Status Register.'' HCLK is AHBCLK The register you want to program is defined by ARM, not ST http://books.google.com/books?id=T9heqSaErCcC&pg=PA147&lpg=PA147&dq=SysTick+Control+and+Status+Register&source=bl&ots=eNvsEdEc5z&sig=fWIFO_tBWbkN_a6-btdbkwiw_-Q&hl=en&ei=4UngS_CKLJTENpTz7c4J&sa=X&oi=book_result&ct=result&resnum=4&ved=0CCMQ6AEwAw#v=onepage&q=SysTick%20Control%20and%20Status%20Registe... The clocks used by ARM are either SYSCLK, or the external clock (in this case ST's HCLK/8). I don't think the HCLK/1 is used, but it would be easy to check. I use HCLK/8, because a 1ms tick doesn't need to be clocking at an excessively high rate SysTick_CLKSourceConfig(SysTick_CLKSource_HCLK_Div8); void SysTick_CLKSourceConfig(u32 SysTick_CLKSource) { /* Check the parameters */ assert_param(IS_SYSTICK_CLK_SOURCE(SysTick_CLKSource)); if (SysTick_CLKSource == SysTick_CLKSource_HCLK) { SysTick->CTRL |= SysTick_CLKSource_HCLK; } else { SysTick->CTRL &= SysTick_CLKSource_HCLK_Div8; } }