cancel
Showing results for 
Search instead for 
Did you mean: 

System Workbench Project Structure Question

carbonefabio
Associate II
Posted on November 23, 2016 at 15:02

Hi, I have a question about the using of System Workbench and projects.

When I download a firmware from ST website, usually I put the extracted folder in the System Workbench workspace, then click Import -> Existing Project Into Workspace (copy project into workspace uncheked).

It works well, but I obtain a project with relative path and liked resource, I mean that the structure of the files that I can see from Eclipse is not the real structure of the files of the folder project. I don't like it, and it confuse me. 

If I want to obtain a ''normal'' structure, I usually copy/paste manually all file in order to recreate the original structure, then I insert include path and symbol. But it is hard and some time leads to compiling errors.

There is a way to do it automatically and safely?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walid FTITI_O
Senior II
Posted on November 29, 2016 at 13:24

Hi carbone.fabio, 

You would check this

http://www.ac6-tools.com/content.php/content_SW4MCU/lang_fr_FR.xphp

for this IDE related request/questions.

-Hannial-