cancel
Showing results for 
Search instead for 
Did you mean: 

SWD clock restrictions

Uwe Bonnes
Chief
Posted on March 06, 2015 at 11:33

Hello,

the STM32 datasheets do not mention any restictions on SWD or JTAG frequency. Some ''internet knowledge'' tells that older ARM cores had a HCLK/6 limitation on SWD/JTAG clock frequency. Has anybody hard facts for Cortex-M and/or STM32?

Thanks

#swclk-limits
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on March 06, 2015 at 11:54

You'd need something pretty exotic to drive it. You might want to ask on an ARM silicon leaning forum. The pins top out at 100 MHz, I'd expect 40-50 MHz to be possible.

http://www.keil.com/ulinkpro/

http://www.arm.com/products/system-ip/debug-trace/coresight-soc-components/serial-wire-debug.php

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
Posted on March 06, 2015 at 12:43

So you postulate that there is no miminum relation between HCLK and SWCLK?

Posted on March 06, 2015 at 14:52

You'd want to find yourself someone familiar with the debug unit implementation, either at ARM or ST, start by pushing in via an FAE.

I'd expect there to be a synchronizer somewhere, which will likely limit you to some fraction of the primary clock, that you're not synchronous with. The logic involved in the shifting is almost certainly capable of >200MHz in an F4.

I don't think it would be that hard to determine where the gears start grinding.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..