cancel
Showing results for 
Search instead for 
Did you mean: 

STSW-LINK009 install

Wu Thomas
Associate II
Posted on September 06, 2017 at 09:21

Hi

I have one set ' P-NUCLEO-53L0A1 '.

It includes: STM32F401 and X-NUCLEO-53L0A1

I download STSW-LINK009 from 

http://www.st.com/en/development-tools/stsw-link009.html

 

And run the

stlink_winusb_install.bat 

with administrative privileges.

Then t

he error messages occur. 

It shows

    1 .ST-Link VCP ctrl device driver  installation unsuccessfully

    2. There is one service installation section is not correct in this INF 

How can I do ?

Thank you.

Operating System: windows embedded standard 2010 service pack 1 (64 bit)

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on September 06, 2017 at 14:53

Hello!

Go to oontrol panel and open the device manager.

 Find the STlink device(the unknown usb device)

right click the device and select properties.

Select Driver tab, then click to the update driver button.

Choose 'browse my compute' for driver software.

And 'Let me pick from a list of device drivers on my computer'

 Browse for the .inf driver file in your unziped stlink folder. Open and push 'Next'.

The driver must be installed.

Imen.D
ST Employee
Posted on September 06, 2017 at 15:09

Hello

mhwuzd

,

This may becaused by incorrectinstallation.

So, try open

Device Manager through'Control Panel' , then right click on 'Properties' for the 'unknown device'.

Click the 'Update Driver' button in the 'Driver' tab to update the driver software,

Then locate and install driver software manually by choosing 'Browse my computer for driver software' to browse the .inf driver file from the unzipped ST-Link folder and click on 'Next'.

Please try this and let me know if your problem is resolved or not.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on September 07, 2017 at 02:27

hi,

I follow your instruction and it shows the same result (with error).

I use the same way to install in another PC (win8)

And the device driver was installed well.

So it should be the OS or PC issue.

But how to solve it?

Posted on September 07, 2017 at 02:28

hi,

I follow your instruction and

it shows the same result (with error).

I use the same way to install in another PC (win8)

And the device driver was installed well.

So it should be the OS or PC issue.

But how

to solve it?