cancel
Showing results for 
Search instead for 
Did you mean: 

How is OSC_OUT connected at HSE bypass source mode?

T YX
Associate
Posted on September 07, 2017 at 05:24

There are two different descriptions in AN2586 and AN1709.

In AN2586 it says it must be left highZ, and as far as I can tell from the figure it means floating.

In AN1709 it says it should be tied to ground.

Does the two means conflict? I think highZ can only be determined by the chip itself and there is nothing I can do with it. So it doesn't matter where it's tied to according to AN2586.

So it's best tied to ground?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0