cancel
Showing results for 
Search instead for 
Did you mean: 

Strange reading over SPI

JulienD
Senior
Posted on May 15, 2015 at 19:15

Hi,

I'm porting an implementation of SD over spi to stm2 using Cube library.

It seems that the communication micro to sd card is ok, it seems that the sd card

answers like it should but it looks like the microcontroler does not interpret correctly

the data on the spi bus.

To get this conclusion, I asked the micro to echo each byte received on SPI to an uart.

On the logic analyzer screen capture joined, you can see :

- on channel 5 (green), data micro -> SD

- on channel 7 (pink), data SD -> micro

- on channel 3 (orange), the uart echo.

Each byte on channel 3 should be the same of the preceeding byte on channel 7 which is

not always the case.

Here's the initialization code of the spi channel :

   __SPI2_CLK_ENABLE();

    GPIO_InitStructure.Pin   = GPIO_Pin_SPI_SD_SCK | GPIO_Pin_SPI_SD_MOSI;

    GPIO_InitStructure.Mode  = GPIO_MODE_AF_PP;

    GPIO_InitStructure.Pull = GPIO_NOPULL;

    GPIO_InitStructure.Speed = GPIO_SPEED_HIGH;

    GPIO_InitStructure.Alternate = GPIO_AF5_SPI2;

    HAL_GPIO_Init(GPIO_SPI_SD, &GPIO_InitStructure);

    GPIO_InitStructure.Pin   = GPIO_Pin_SPI_SD_MISO;

    GPIO_InitStructure.Mode  = GPIO_MODE_INPUT;

    GPIO_InitStructure.Pull = GPIO_PULLUP;   // obligatoire

    HAL_GPIO_Init(GPIO_SPI_SD, &GPIO_InitStructure);

    /* SPI configuration */

    hndSPI.Instance = SPI_SD;

    hndSPI.Init.Mode = SPI_MODE_MASTER;

    hndSPI.Init.Direction = SPI_DIRECTION_2LINES;

    hndSPI.Init.DataSize = SPI_DATASIZE_8BIT;

    hndSPI.Init.CLKPolarity = SPI_POLARITY_LOW;

    hndSPI.Init.CLKPhase = SPI_PHASE_1EDGE;

    hndSPI.Init.NSS = SPI_NSS_SOFT;

    hndSPI.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16; // 72000kHz/256=281kHz < 400kHz

    hndSPI.Init.FirstBit = SPI_FIRSTBIT_MSB;

    hndSPI.Init.TIMode = SPI_TIMODE_DISABLED; // todo valeur au hasard = motorola, sinon TI

    hndSPI.Init.CRCPolynomial = 7;

    hndSPI.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;

    HAL_SPI_Init(&hndSPI);

Here's how I read over it :

BYTE rcvr_spi() {

    uint8_t rx;

    uint8_t tx = 0xff;

    HAL_SPI_TransmitReceive(&hndSPI, &tx, &rx, 1, 50);

    HAL_UART_Transmit(&huart4, &rx, 1, 50);

    return rx;

}

Does anybody have an idea of what could be wrong ?

Regards

Julien
This discussion is locked. Please start a new topic to ask your question.
22 REPLIES 22
JulienD
Senior
Posted on May 29, 2015 at 11:40

And another question:

OSPEED

Rx are used for output pins and the logic analyzer has shown that the output

was correct (without ambiguity regarding the sampling rate vs SPI frequency). Reading wasn't...

How is this possible ?

waclawek.jan
Super User
Posted on December 05, 2015 at 03:25

I've just seen this bug being described in the brand new STM32F410's errata, dated September 2015. Its description is not that straightforward, and the erratum's title reflects this: ''LSB bit of data or CRC calculation can be corrupted for the received

data in master mode depending on the timing of the feedback

communication clock respect to the APB clock (SPI or I2S)''

I guess this impacts ALL STM32 SPI incarnations up to date - I may be wrong of course, but this is a recurrent topic here with various STM32 families for years, just follow the links and google. It will take some time and maybe also some influential customers' screaming until it propagates into the errata for all the related chips.

JW

Imen.D
ST Employee
Posted on September 21, 2016 at 10:54

Hello waclawek.jan,

Thank you for highlighting this issue.

Please note that your feedback is reported internally to take the necessary action and update Errata Sheet in coming version.

Sorry for the inconvenience it may bring.

Best Regards

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen