cancel
Showing results for 
Search instead for 
Did you mean: 

Strange behavior of Port G and SPI of STM32L4+ (STM32L4R7ZIT6-144 Pin LQFP Package)

VK Verma
Senior
Posted on May 19, 2018 at 06:04

Hi !

I am using STM32L4R7ZIT6-144 Pin LQFP Package on Keil-MDK, So far all other GPIO ports SET/REST test is normal except Port G with its associated SPI configuration which is neither getting SET nor RESET on push pull ,pull up mode. Although System viewer during debug mode in Keil -MDK showes normal set/reset toggle behavior for PG9/10/11/12 ports but output of the ports is not remains low and unchnaged.

I have tested VDDIO supply at pin no 131 and 95 with respect to 130 and 94 which is 3.2V.

We have tested it with three different hardware's and found the behavior same.

Due to this we are unable to use SPI3 on either of these ports.

Please advice!

Thanks and Best Regards,

VK Verma   

‌

https://community.st.com/tags♯/?tags=stm32l4%2B

‌

#stm32l4r7zit6 #stm32l4+
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on May 19, 2018 at 06:14

Haven't tried for SPI, but for UART on Port G you have to enable the VDDIO2 supply

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4
Posted on May 19, 2018 at 06:14

Haven't tried for SPI, but for UART on Port G you have to enable the VDDIO2 supply

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 19, 2018 at 06:39

    /* IOSV bit MUST be set to access GPIO port G[2:15] */

    __HAL_RCC_PWR_CLK_ENABLE();

    HAL_PWREx_EnableVddIO2();
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 19, 2018 at 06:35

Hi Clive,

I appreciate your experience and your observation was right.

After enabling VDDIO2 both SPI and ports G are working normal.

It was very device specific function.

Once again thanks for your support.

Regards,

VK Verma  

Posted on May 19, 2018 at 08:45

HI !

Noted and problem resolved.

Thanks and Once again!

Thanks and Best Regards,

VK Verma