cancel
Showing results for 
Search instead for 
Did you mean: 

Storing variable in Flash memory

mani s
Associate III

I can store variables in flash memory location successfully but what is happening is updating that variable in main.c file not happening.I'm posted code what i have done below. 

Linker script file :

MEMORY

{

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K

FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 153

MY_VARS (xrw) : ORIGIN = 0x08005000, LENGTH = 1K // storing in flash memory

}

.my_vars :

{

*(.MY_VARS*);

} >MY_VARS

In main.c file :

__attribute__((section(".MY_VARS"),myvars)) uint32_t *value=8;

int main()

{

int a =sum(); //i have a sum function of two numbers and storing in variable 'a'

value =&a; // value should updated to sum but it is not updating

readaddress=(const volatile uint32_t *)0x08005000;// reading flash memory 

printf("Read flash address %lu\n",*readaddress);// printing the data which is stored in value ,it is printing everytime 8 but it should print variable data which stored in 'a'.

}

int sum(int a)

{

int a=1, b= 34 ;

a=a+b;

return a;

}

Can anybody help me to figure this out,i hope u understood what im asking.

Thank you

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

You could use a function pointer. The address of the function should be ODD. Confirm it's placement by reviewing the .MAP file

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Community member​  can you elaborate the answer ?

My understand is ,to create a fun pointer in the flash and excess from the project-2.

what do you mean by ODD ? why it should be odd.

Odd as in not even. Thumb instruction addresses are designated as odd due to the way the microcontroller decodes them. ie 0x08004001​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..