Skip to main content
Associate
Apr 29, 2026 12:20 PM UTC
Solved

X-CUBE-EEPROM doesn't update variable

Hello,

I am using X-CUBE-EEPROM as a mean to store variable in internal FLASH memory on STM32U5G9-DK2 board. Here is my function where a variable in flash:

static FLASH_STATUS flash_slot_write_shared_key(const FLASH_INDEX *index, uint8_t slot, uint8_t *shared_key) {
	if (slot > FLASH_SLOTS_NUMBER)
		return FLASH_WRONG_PARAM;

	if (shared_key == NULL)
		return FLASH_NULL_PARAM;

	EE_Status ee_status = EE_WRITE_ERROR;

	HAL_FLASH_Unlock();
	taskENTER_CRITICAL();
	ee_status = EE_WriteVariable96bits((uint16_t)index->entries[slot].addr, (uint64_t *)(shared_key));
	if (ee_status != EE_OK)
		return FLASH_ERROR;
	ee_status = EE_WriteVariable96bits((uint16_t)index->entries[slot].addr + 1, (uint64_t *)(shared_key + 12));
	if (ee_status != EE_OK)
		return FLASH_ERROR;
	ee_status = EE_WriteVariable32bits((uint16_t)index->entries[slot].addr + 2, *(uint32_t *)(shared_key + 24));
	if (ee_status != EE_OK)
		return FLASH__ERROR;
	ee_status = EE_WriteVariable32bits((uint16_t)index->entries[slot].addr + 3, *(uint32_t *)(shared_key + 28));
	if (ee_status != EE_OK)
		return FLASH_ERROR;
	taskEXIT_CRITICAL();

	HAL_FLASH_Lock();

	return FLASH_OK;
}

 Here is the function to read back the variable:

static FLASH_STATUS flash_slot_get_shared_key(const FLASH_INDEX *index, uint8_t slot, uint8_t *shared_key) {
	if (index == NULL || shared_key == NULL)
		return FLASH_NULL_PARAM;

	if (slot > FLASH_SLOTS_NUMBER)
		return FLASH_WRONG_PARAM;

	EE_Status ee_status = EE_WRITE_ERROR;

	uint8_t tmp[32] = {0};
	memset(tmp, 0, 32);

	HAL_FLASH_Unlock();

	HAL_ICACHE_Invalidate(); // TODO: Configure MPU

	ee_status = EE_ReadVariable96bits((uint16_t)index->entries[slot].addr, (uint64_t *)tmp);
	if (ee_status != EE_OK)
		return FLASH_ERROR;
	ee_status = EE_ReadVariable96bits((uint16_t)index->entries[slot].addr + 1, (uint64_t *)(tmp + 12));
	if (ee_status != EE_OK)
		return FLASH_ERROR;
	ee_status = EE_ReadVariable32bits((uint16_t)index->entries[slot].addr + 2, (uint32_t *)(tmp + 24));
	if (ee_status != EE_OK)
		return FLASH_ERROR;
	ee_status = EE_ReadVariable32bits((uint16_t)index->entries[slot].addr + 3, (uint32_t *)(tmp + 28));
	if (ee_status != EE_OK)
		return FLASH_ERROR;

	HAL_FLASH_Lock();

	memcpy(shared_key, tmp, 32);

	return FLASH_OK;
}

Once I write a key to the defined slot, if I try to update it, I still get the first written value in memory. How I am supposed to update the variable. Am I misusing the API ?

Chloe Meunier
Chloe MeunierBest answer
ST Employee
Apr 30, 2026 9:45 AM UTC

Hello,

 

On AN4894  https://www.st.com/resource/en/application_note/an4894-how-to-use-eeprom-emulation-on-stm32-mcus-stmicroelectronics.pdf the data update flow is described  in Figure 5.

If you update a variable, the first value of this variable is still written in flash as long as the first page is not full.

 

BR

Chloé

1 reply

Chloe Meunier
Chloe MeunierBest answer
ST Employee
Apr 30, 2026 9:45 AM UTC

Hello,

 

On AN4894  https://www.st.com/resource/en/application_note/an4894-how-to-use-eeprom-emulation-on-stm32-mcus-stmicroelectronics.pdf the data update flow is described  in Figure 5.

If you update a variable, the first value of this variable is still written in flash as long as the first page is not full.

 

BR

Chloé