2016-08-27 12:00 AM
Hello All ;
I am sorry if it is not the right forum to post ; In my project I need a wifi connection ;My question : is how to choose the best wifi module of my application : we see that ST has a good wifi modulehttp://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.html
; and we have other option esp8266 but what is the advantage of each ? Anyone uses both could tell me the advantages of each please ? Thank you inadvantage2016-08-30 5:32 AM
Any support here , please ?
2016-08-30 5:41 AM
Depends on your application.
With the SPWF01SA you need also an extra cpu. I prefer the Esp8266, with Arduino ide you have it up and running in 10 minutes. And also important there's a big community out there who can help you.2016-08-30 6:49 AM
Hi,
You can refer to the and this which explain why to use SPWF01S Series. Maybe this is interesting for you. Regards2016-12-27 7:41 PM
looking at the STM32F103REY6 chip on the SPWF01SA, it has 3 SPI's. Are all 3 of these available to be programmed (I don't see them mentioned in the datasheet) or is it possible to use one of the SPI's MOSI/MISO,SCLK pins and then just use 3 separate GPIO's for the chip select CS pin for my 3 slaves? I need to be able to run 3 SPI slaves, a 20x4 LCD screen and 3 triac relays thru optoisolators. Is my SPI config possible on this chip/wifi module to get what I need out of it plus the wifi features or do I need to run another MCU along side this chip to do all this?