2021-08-11 2:26 AM
Hi,
I have used the Cube IDE to generate project code for a STM32WL55JC1 (Dual Core). I have activated FreeRTOS for the M4 core (cpu1). The generated code places the call to release the M0+ core (cpu2) after the kernel has been handled control (unreachable code). Is this a bug or am I missing something here?
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Boot CPU2 */
HAL_PWREx_ReleaseCore(PWR_CORE_CPU2);
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */Thanks
Mark
2021-08-11 4:41 AM
Yeah seems like it's in the wrong order. It isn't that way in the examples.
2021-08-11 4:54 AM
Thanks, thought so, I placed a call to release the core just before FreeRTOS get initialized.