2015-08-12 11:52 PM
Hello everyone.
I am building a simple car audio/video player, and the 429i with the LCD built into it seems perfect. I want to use a different DAC, specifically Ti's PCM5122, so that I can use higher grade amps, among other things. I've nutted out the DAC config (not as simple as it sounds, it's quite a powerful part), but when I fire up CubeMX and tell it I'm using a 429 disco kit it won't give me access to any of the I2S busses onboard. I havn't got the 429 kit yet, it's in the mail, but I would like to know if I can access an i2s and i2c bus while still using the LCD. I can't find anything in the documentation about this, and a search here bought up nothing.Has anyone else had this issue? or is CubeMX just messing with me? Thank you :)2015-08-13 9:57 AM
The
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00093903.pdf
should breakdown very clearly the pins used/unused in the design. It's not a very expandable/extensible board because of the low pin count device used, and the number of pins soaked up by the SDRAM + LCD.Review the ''Free IO'' column, and what on the board you can remove/discard.