2016-02-10 1:11 AM
Hi,
I'm trying to get comms between USART1 and USART6 working. I can send from USART1 to USART6 using interrupts and it works. What I am trying to do now is control the sending interrupt, but I think I am missing something. So the IRQ1handler just goes through a send buffer and send data, great no problem, but I cannot seem to stop it. This is my IRQ1Handlervoid USART1_IRQHandler(void)
{
if (USART_GetITStatus(USART1, USART_IT_TXE) != RESET) // Transmit the string in a loop
{
USART_SendData(USART1, StringLoop[tx_index++]);
if (tx_index >= BUFFER_SIZE)
{
tx_index = 0;
USART_ITConfig(USART1,USART_IT_TXE,DISABLE); //When all data received, stop interrupt for TXE flags
}
}
}
and this is my main
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
NVIC_USART1_Configuration();
NVIC_USART6_Configuration();
USART1_Configuration();
USART6_Configuration();
while (1)
{
Delay(2000);
USART_ITConfig(USART1,USART_IT_TXE,ENABLE);
}
}
So basically I am trying to enable the transmission every 2 seconds, not continuously send it.
Any advice would be appreciated. Thanks
2016-02-10 3:17 PM
Dembek, thank you for encouragement (virtual kick in the a*s) - it worked.
Got my main sortedint main(void)
{
RCC_Configuration();
GPIO_Configuration();
NVIC_USART1_Configuration();
NVIC_USART6_Configuration();
USART1_Configuration();
USART2_Configuration();
USART6_Configuration();
while (1)
{
USART_ITConfig(USART1,USART_IT_TXE,ENABLE);
Delay(0xFFFFF);
Delay(0xFFFFF);
Delay(0xFFFFF);
Delay(0xFFFFF);
}
}
The TX IRQ really hasn't changed. By adding these delays in the main I can see in debug a much longer delay until the RX buffer fills up (I am not losing any data). I guess my next step will be to implement some sort of more sensible control when i want data to be sent and when not.
What would be a typical pattern in implementing interrupt driven TX? Circular buffer?
Thanks
2016-02-11 1:16 AM
OK. Specially for You.
#define buffer_size 256 //!< Buffer size for USART1 (must be power of 2)
#define buffer_mask (buffer_size - 1) //!< Mask for buffer indexes for USART1.volatile char RXD1_buffer[buffer_size]; //!< Input buffer for USART1.
volatile char TXD1_buffer[buffer_size]; //!< Output buffer for USART1. volatile uint32_t RXD1_head; //!< Head of input buffer for USART1. volatile uint32_t TXD1_head; //!< Head of output buffer for USART1. volatile uint32_t RXD1_tail; //!< Tail of input buffer for USART1. volatile uint32_t TXD1_tail; //!< Tail of output buffer for USART1.void USART1_IRQHandler(void)
{ uint32_t tmp; if (USART1_SR_RXNE_bb) { tmp = RXD1_head; RXD1_buffer[tmp] = USART1->DR; RXD1_head = (tmp + 1) & buffer_mask; if (RXD1_head == RXD1_tail) { // buffer overflow detection } } if (USART1_CR1_TXEIE_bb && USART1_SR_TXE_bb) { tmp = TXD1_tail; if (TXD1_head != tmp) { tmp = (tmp + 1) & (buffer_size - 1); USART1->DR = TXD1_buffer[tmp]; TXD1_tail = tmp; } else { USART1_CR1_TXEIE_bb = 0; } } } void USART1_SendString(const char *s) { char c; uint32_t tmp_head; while ((c = *s++)) { tmp_head = (TXD1_head + 1) & buffer_mask; while (tmp_head == TXD1_tail); TXD1_buffer[tmp_head] = c; TXD1_head = tmp_head; } USART1_CR1_TXEIE_bb = 1; }2016-02-11 12:10 PM
Radoslaw,
This is great, I actually understand the logic and can make sens off it. Thank you for this, much appreciated.