cancel
Showing results for 
Search instead for 
Did you mean: 

STM32W108 + Flash Programming error

shaktishekhar789
Associate II
Posted on July 02, 2013 at 08:44

Hello

    I am using IAR embedded workbench tool and STM32W108XX device for development purpose. When I program it I got error message as

  No reply received.. 

  Error while initializing interface.

Please help me asap..

#clive1
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on July 02, 2013 at 14:19

I'm not a user of IAR or W1 parts. This doesn't look to be a message from IAR using SWD/JTAG

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Nickname306_O
Senior
Posted on July 03, 2013 at 12:43

Could you please give us further details? the example you are runnig ? the RF board you are using ?

shaktishekhar789
Associate II
Posted on July 03, 2013 at 17:23

I am running emberZnet stack on STM32W108CC RF kit. I am programming it through command window using flasher command...

Posted on July 03, 2013 at 17:52

These boards?

http://www.st.com/web/en/catalog/tools/PF251361

Are you should you have the STM32W108 in a flashable mode?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
shaktishekhar789
Associate II
Posted on July 03, 2013 at 19:29

Yes. This is the board I am working on.I have programmed it number of times before it. But now I am getting such type of error..