cancel
Showing results for 
Search instead for 
Did you mean: 

STM32vldiscovery and hd44780 display

joesoftware
Associate II
Posted on October 31, 2012 at 20:26

Hi, i tried to use IAR example about LCD for use my display hd44780.

I connected 6 pin (RS,E,DB4,DB5,DB6,DB7) for use it on 4bit configuration (i'm sure that the connection is good cause i used that on my old arduino board).

I only see first line of black simple, nothing else.

Can someone help me with that code or link some other library that work good on stm32vldiscovery.

Thx
This discussion is locked. Please start a new topic to ask your question.
23 REPLIES 23
joesoftware
Associate II
Posted on November 11, 2012 at 19:24

I just can link u this

http://joshuagalloway.com/lcd.html

, i see that some value is different from ur project, i hope it is helpful for u.

joesoftware
Associate II
Posted on November 14, 2012 at 18:49

I used the link before for rewrite my code, and it run good for 4bit configuration, if u haven't solved ur problem yet i can give u my code.

Bye

orn
Associate II
Posted on November 15, 2012 at 09:05

I'm working on 8-bit, I have not adjusted the controls 4-bit, if you give me your code I check where is my error! thanks.

joesoftware
Associate II
Posted on November 15, 2012 at 09:56

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6mL&d=%2Fa%2F0X0000000bvD%2FU8jBT1ZDmrorlBjsUgGtv.Cz7Evh3C5YF9Skijcnxmg&asPdf=false