Skip to main content
Associate
July 1, 2024
Question

STM32U5F display resolution

  • July 1, 2024
  • 2 replies
  • 938 views

Hello,

I read the AN4861 and try to determine the max LCD resolution for a STM32U5F without using external RAM. The lowest color is 16 bit, RGB656. 

I would like to use 1366*768, which should be 1049088 pixel, this should approx 1.9MB for the framebuffer. 

 

Would this work ?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
July 1, 2024

Bandwidth should be fine, DSI 2-Lane was one of the constraints to 1.1 - 1.2 Mpixel ceiling

Generally you'd prefer to have two frame buffers so there's less disruption / tearing due to you painting into an active buffer

62.5 MHz -> 1366x768 at 60 Hz

Frame buffer a little over 2MB

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MartinNPNAuthor
Associate
July 2, 2024

thanks for the fast answer.

 

I thought the bandwith should be fine, but i would like to use LTDC with a RGB interface and not DSI. which should work too, or ?

For me would 50Hz be fine too. 

 

The STM32U5F has 3MB RAM, which should be ok, if i get the datasheet right the LTDC can work with different RAM banks as the larger banks are only 800kB.