cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5 LL example ADC1 and ADC4

edw
Associate

The example project does not provide information on ADC4 register configurations, ADC4 seems to be different then prior peripherals (e.g. compared to L4).  

...\NUCLEO-U575ZI-Q\Examples_LL\ADC\ADC_SingleConversion_TriggerSW_IT_Init

STM32CubeMX configuration tool is close, but does not generated completely working examples (not for me at least).

Merging the two together, I created the attached example (crude but functional).

change these two #define's in main.h to switch ADC peripheral ADC1(2) or ADC4

  #define MY_ADC_TYPEDEF ADC1 //ADC1 or ADC4

  #define MY_ADC_IRQHandler ADC1_IRQHandler //ADC1_IRQHandler or ADC4_IRQHandler

 

enjoy, hope this helps someone get started with the ADC4 peripheral on the STM32U5

 

note: the post only allowed three files

stm32u5xx_it.h

requires this addition, based on the #define in main.h

/* USER CODE BEGIN EFP */

void MY_ADC_IRQHandler(void);

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0