2025-12-23 10:00 PM
Hello,
I would like clarification on the behaviour of STM32U3 devices when Readout Protection (RDP) Level 1 is enabled.
Configuration:
TrustZone: Disabled
Debug interface: SWD/JTAG
Questions:
With RDP Level 1, is Flash completely unreadable by any third-party tool or by any boot mode (system memory boot, RAM boot, etc.), except when accessed by application code running on the MCU?
With RDP Level 1, is application debugging still supported (attach debugger, halt, step, breakpoints), and are there any known limitations compared to RDP Level 0?
Any confirmation or documentation reference would be appreciated.
Thank you,
Vijay