2026-02-26 9:03 AM - last edited on 2026-04-28 7:18 AM by Andrew Neil
Split from original question
Can you check your documentation ? According to RM086 - Reference Manual for STM32N657, all PH GPIOs can be set as input/output (contradicting your previous post).
Please retest your device and determine which document is correct.
thanks
Matthew
2026-04-28 7:13 AM
Hi @matt-crc
On STM32N6, PH0 and PH1 are input only as indicated in datasheet not like other products. Actually, these are limited to 1.8V instead of 3.3V
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.