2025-06-25 6:35 AM - last edited on 2025-06-25 7:23 AM by Andrew Neil
Tried to erase , recently i keep getting this error ,
when attempting to erase through IDE even though not successful , after several tries it programs.
2025-06-25 8:01 AM
Ok, but no one here is familiar with the specifics of your board design. Provide MORE contextual detail.
How do you have this wired to the ST-LINK, is NRST connected?
Any watchdog on the board, that might break the connection?
Does pulling BOOT0 HIGH help with making a connection?
Issues with Power on the board, a brown-out might cause the chip to reset / stop responding.
2025-06-25 9:14 AM - edited 2025-06-25 9:33 AM
J3 is where i am having trouble, as mentioned it deosnt happen always.
the option bytes shows the read protection/write protection has not been enabled.