cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L562QEI6 OPAMP Input pin floating?

MFail.11
Associate III

Hello,

I'm working with STM32L562QEI6 mcu for a project.

I don't need OPAMP so it will be disabled by software, but on the PCB can I leave the pins floating or connected to ground?

There are two OPAMP input pins and they are dedicated, they can't be GPIO.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen GH
ST Employee

Hello @MFail.1​ ,

It would be better to not put the pins floating  

So, it should be connected to GND.

Imen

MFail.11
Associate III

Thanks,

but should work also with that pin floating, right?