2017-04-19 12:27 AM
Hello,
I want to use DFU for update my program on the STM32L476RG. I use a personnal board. When I put BOOT0 to VCC, the Bootloader start and we can change the firmware but my system is on battery and I have no access to BOOT0 pin and RESET.
So I want to jump in bootloader directly from software for that I have search the start addresse of system memory of the MCU -> 0x1FFF0000. So this is my code :
#define USBD_DFU_APP_DEFAULT_ADD 0x1FFF0000
pFunction JumpToApplication;
uint32_t JumpAddress;
/***
**** some code HERE
***/
HAL_RCC_DeInit();
HAL_DeInit();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
//_HAL_REMAPMEMORY_SYSTEMFLASH();
/* Jump to user application */
JumpAddress = *(__IO uint32_t*) (USBD_DFU_APP_DEFAULT_ADD + 4);
JumpToApplication = (pFunction) JumpAddress;
/**
* Step: Disable all interrupts
*/
__disable_irq();
__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) USBD_DFU_APP_DEFAULT_ADD);
JumpToApplication(); �?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
When I use this code the system reset but not in DFU mode. What I have miss for do a good reset DFU ?
I have try theUSBD_DFU_APP_DEFAULT_ADD to 0x00000000 no change.
Thanks,
Loïc
Solved! Go to Solution.
2017-04-24 2:52 AM
Thanks
and !! Finally I find the solution for jump to bootloader !Yes it's the barriers the solution.
This is my finally code, I hope it will help someone else :
typedef void (*pFunction)(void);pFunction JumpToApplication;uint32_t JumpAddress;HAL_RCC_DeInit();SysTick->CTRL = 0;SysTick->LOAD = 0;SysTick->VAL = 0;/** * Step: Disable all interrupts */__disable_irq();/* ARM Cortex-M Programming Guide to Memory Barrier Instructions.*/__DSB();__HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH();/* Remap is bot visible at once. Execute some unrelated command! */__DSB();__ISB();JumpToApplication = (void (*)(void)) (*((uint32_t *)(0x1FFF0000 + 4)));/* Initialize user application's Stack Pointer */__set_MSP(*(__IO uint32_t*) 0x1FFF0000);JumpToApplication();�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Thanks again !
Loïc
2017-04-26 1:54 PM
Very helpful! I've been dealing with HardFault's for days now. This was the key.
Thank you!
- SteveK
2017-10-19 6:32 AM
Hi.
I use this code, but have HardFault ((
Please show your code!
2017-10-19 7:28 PM
Hi Alexsandr,
Here's the code I used for the ST32L052.
Steve
-------------------------------------------------------------
void upgradeFirmware(void)
{ void (*JumpToBootloader)(void); uint32_t msp; // Disable all IRQs HAL_NVIC_DisableIRQ(SysTick_IRQn); HAL_NVIC_DisableIRQ(USART1_IRQn); HAL_NVIC_DisableIRQ(DMA1_Channel1_IRQn); __disable_irq();// Disable used PLL
HAL_RCC_DeInit(); SysTick->CTRL = 0; // Reset the Systick Timer SysTick->LOAD = 0; SysTick->VAL = 0; // Set the main stack pointer msp = 0x1FF00000; JumpToBootloader = (void (*)(void))*(uint32_t*)0x1FF00004;// goto the bootloader, we won't be coming back from here...
*(__IO uint32_t *)FWUG_MAGIC_NUMBER_ADDR = 0x12348765; // Set the magic number for when we reboot after unlocking sectors __set_MSP(msp); JumpToBootloader();while (1);
}
------------------------------------------
2024-04-19 4:51 AM
It works, thanks.