cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L476G-Disco LSE Startup Problem

gokhannsahin
Associate II
Posted on January 05, 2018 at 14:44

Hi everyone,

I want to use RTC module and LSE crystal which is default on board 32768KHz. I generate the code via STM32Cube because I couldn't find any example of RTC that used via LSE. After generated, the code doesn't pass the LSE ready check. I guess the reason for that issue isn't hardware because the code is running on discovery board. I have tried firmware 1.10 and 1.9 libraries for stm32l4 but the result is same. Where am I doing wrong?

#stm32l476-discovery-board #lse-startup
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on January 09, 2018 at 12:50

Luckily you can use other sources of the clock for RTC...