STM32L476 RTC with SuperCap
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-14 1:34 AM
Hi everyone,
Should I connect a any series resistor to the super capacitor while using a super capacitor that is 1F 5.5V instead of a battery? Or I can connect directly the capacitor to VBat pin?
#power-backup-supercapacitor-rtc #rtc- Labels:
-
RTC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-02-15 10:22 PM
oops, forgot to calc in the diode to stop reverse current back to the power supply..
since we have to charge the Supercap with a diode, the Supercap voltage will sit at 2.7V when charged.
recalculating;
V=IR. we can drop 2.7 - 1.8 = 0.9V before the RTC input voltage is below spec.1.8V
R = V/I 0.9 / 35e-6 = 25k7 R needed in series (maximum)
if you use a 22k, R will drop 22k x 35e-6 = 0.77v across the resistor.
the pin should sit at 2.7 - 0.77 = 2V, after power off is ok, above 1.8v
22K should be great....
sorry for the after thought....
otherwise, I think you may want to replace that processor, it may be already damaged.
:(

- « Previous
- Next »