cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L433: can't make sense of Flash Loader Demonstrator

Peter Mather
Associate III

During development I've been using ST-LInk to program the STM32L433 which of course works perfectly. I want to release the firmware and allow users to be able to update the code over UART2.

I've set BOOT0 and can see the device using the latest version of the STM Flash Loader Demonstrator program (V2.8.0). It reports PID = 435, BID = NA, Version 3.1. The flash mapping panel is completely blank. It says it is read protected although I haven't set any protection.

I can use the option to disable read protection and this seems to work - I get the message "Read protection was successfully removed" but if I try to read the chip it again says it is read protected. If I try and erase or write the chip I always get the read-protected message.

I'm missing something as usual but what?

Help gratefully appreciated

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Use the STM32 Cube Programmer, it has a USART mode, the old software is deprecated/abandoned.

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

1 REPLY 1

Use the STM32 Cube Programmer, it has a USART mode, the old software is deprecated/abandoned.

https://www.st.com/en/development-tools/stm32cubeprog.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..