cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432 - HSI16 accurate enough for use without crystal?

mluessi
Associate II
Posted on December 30, 2017 at 16:23

I started designing a product with a STM32L432KCU6. Looking at the datasheet I noticed that the HSI16 clock seems to be very accurate. From Figure 14, p 95, it seems that the clock is pretty much within 16MHz +/- 1.5% for the -20C to 100C range. In comparison, for older parts (e.g. F405) the HSI clock is +/- 4% for the -10C to 85C range.

Does anyone know if this is accurate? It seems to me that this means I shouldn't have to use an external crystal, which would be nice as it reduces cost and board space, and also frees up some IOs . I plan to use UARTS with bit rates up to 115kbps, but a clock variation of 1.5% should be OK for this.

Thoughts?

#stm32l4
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on December 30, 2017 at 16:44

For something to be 'accurate' you'd look for numbers in ppm or ppb, not percentages.

Serial UART can be very sloppy (+/-5% or worse), where you need accurate clocks are Ethernet, USB and CAN

Crystals, which might be off in frequency, don't vary second-to-second in the way you're likely to observe RC sources.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mluessi
Associate II
Posted on December 30, 2017 at 16:57

Thanks for the input! I will be using USB as well, but the HSI48 can be adjusted based on the USB clock (clock recovery circuit), which is intended to enable crystal-less operation.

So, do you think HSI16 will be good enough for UART communication or should I be worried about the '

second-to-second

 frequency variation' you mentioned? 

Posted on December 30, 2017 at 17:44

High Speed USB expects +/-500ppm (0.05%)

I would avoid crystal-less USB, you save a few cents on the design at the expense of having a product viewed as unreliable, and with high support costs.

Serial UART can tolerate a lot of bit clocking error, easily more than 5% in OVER16 mode, so the HSI or MSI sources should have no problem

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..