cancel
Showing results for 
Search instead for 
Did you mean: 

stm32L432(32 QFN) usart2 + lpuart tx possible?

isjeon
Associate II
Posted on June 21, 2018 at 20:35

Hi,

With the cubeMx tool, when i use usart2 , the lpuart can not be included.

But when i set as bellow, is it possible to use usart2 tx/rx full duplex, and lpuart tx only ?

-- as follows--

Usart2

TX : PA2

RX: PA15

LPUART

TX : PA3

RX : 

(!! with pin swap option)

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 21, 2018 at 20:45

The GPIO and AF settings should be able to achieve that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..