cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 opamp to ADC constraints

Yan M??roth_O
Associate
Posted on January 11, 2018 at 17:21

Hi,

My stm32 opamp characteristics understanding is that

- max output current 500µA in normal mode, stand-alone

- min output impedance 4kR in normal mode, stand-alone.

This last value fairly aligns to considering a serviceable output impedance corresponding to 3.6V/2 / 500µA.

As a consequence, when one routes opamp output (standalone+normal mode) into ADC input, it means that sample rate should a Rain above 4k. Do i get it right?

For example, for ADC running at 80MHz and 12 bit resolution :

  • (fast channel) min usable Rain_max = 4,7k

    Corresponds to selecting min 92.5 sampling cycles

    Results in anti-aliasing required cut-off at Fs/2 = ~380kHz max
  • (slow channel) min usable Rain_max = 10k

    Corresponds to selecting min 247.5 sampling cycles

    Results in anti-aliasing required cut-off at Fs/2 = ~154kHz max

Regards,

Y.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0