cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L152 RTC periodic wakeup

matteo239955
Associate III
Posted on November 05, 2013 at 14:42

Hi all,

I'm quite new with STM32 and I'm trying to set up the RTC module to raise a periodic wake-up interrupt every second (using LSI).

The configuration seems to be working, the interrupt is effectively raised, but the firmware is blocked inside the library function ''RTC_GetITStatus'' and loops inside it.

The code in that moment is running with Interrupt ''priviledges'' and the result is that the whole firmware is ''bloked''.

This is the code I'm using... can anybody tell-me how to unlock the situation?

/**********************************************************************/

void RTC_Config()

{

NVIC_InitTypeDef NVIC_InitStructure;

EXTI_InitTypeDef EXTI_InitStructure;

/* Enable the PWR clock */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);

  /* Allow access to RTC */

  PWR_RTCAccessCmd(ENABLE);

    

  /* Enable the LSI OSC */ 

  RCC_LSICmd(ENABLE); // The RTC Clock may varies due to LSI frequency dispersion

  /* Wait till LSI is ready */  

  while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET);

  /* Select the RTC Clock Source */

  RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);

  

/* Enable the RTC Clock */

  RCC_RTCCLKCmd(ENABLE);

  /* Wait for RTC APB registers synchronisation */

  RTC_WaitForSynchro();

/* EXTI configuration *******************************************************/

  EXTI_ClearITPendingBit(EXTI_Line20);

  EXTI_InitStructure.EXTI_Line = EXTI_Line20;

  EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;

  EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;

  EXTI_InitStructure.EXTI_LineCmd = ENABLE;

  EXTI_Init(&EXTI_InitStructure);

// Configuring RTC_WakeUp interrupt

  NVIC_InitStructure.NVIC_IRQChannel = RTC_WKUP_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

// RTC Wakeup Configuration

RTC_WakeUpClockConfig(RTC_WakeUpClock_CK_SPRE_16bits);

// RTC Set WakeUp Counter

RTC_SetWakeUpCounter(0);

// Enabling RTC_WakeUp interrupt

RTC_ITConfig(RTC_IT_WUT, ENABLE);

// Disabling Alarm Flags

RTC_AlarmCmd(RTC_Alarm_A, DISABLE);

RTC_AlarmCmd(RTC_Alarm_B, DISABLE);

// RTC Enable the Wakeup Function

RTC_WakeUpCmd(ENABLE);

}

/**********************************************************************/

void RTC_WKUP_IRQHandler(void)

{

if(RTC_GetITStatus(RTC_IT_WUT) != RESET)

{

RTC_ClearITPendingBit(RTC_IT_WUT);

GPIO_ToggleBits(LD4_GPIO_PORT, LD4_PIN);

}

}

/**********************************************************************/

Thanks a lot!

#stm32l-rtc-autowakeup-timer #interrupts
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on November 05, 2013 at 14:58

void RTC_WKUP_IRQHandler(void)
{
if(RTC_GetITStatus(RTC_IT_WUT) != RESET)
{
RTC_ClearITPendingBit(RTC_IT_WUT);
EXTI_ClearITPendingBit(EXTI_Line20); // And EXTI
GPIO_ToggleBits(LD4_GPIO_PORT, LD4_PIN); 
}
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
matteo239955
Associate III
Posted on November 05, 2013 at 15:01

Thank you very mutch clive1!