cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l151c8t6a device marking with QR code

owen_chen
Associate

Hi, I bought 50pcs STM32L151C8T6A from one Chinese online vendor, which has device marking with QR code.

I encountered an issue while using the new version chip, after initial power-on, the overall sleep current of the product is approximately 5uA(STM32L151C8T6A in stop mode), When I reset the product's hardware multiple times, there is a high probability that the product's sleep current will reach up to 1.6mA. Once this occurs, the product can only return to normal by being powered on again.

With the same hardware, replacing the STM32L151C8T6A with an older version will prevent the issue from occurring.

This is a mature product, and this is also my first time using the new version of STM32L151C8T6A. Is the software for the old and new versions incompatible? What should I be aware of?

ps: I am using the STM32L series standard library.

 

 

owen_chen_0-1763653398218.png

 

owen_chen_1-1763653463367.png

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @owen_chen and welcome to the ST community,

I recommend to contact your local ST sales/FAE for that.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello @owen_chen and welcome to the ST community,

I recommend to contact your local ST sales/FAE for that.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.