cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151 stack width

nanayakkaraan
Associate II
Posted on April 19, 2012 at 11:43

Dear all,

What is the stack width of STM32L151r8?

Thank you
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
frankmeyer9
Associate II
Posted on April 19, 2012 at 11:58

Not sure what you mean.

The stack is placed in RAM, and is 32 bit wide in an 32 bit architecture like CM3.

The stack size is purely a property of your toolchain / application, as it is just some reserved RAM, with the stack pointer pointing to the begin.

nanayakkaraan
Associate II
Posted on April 20, 2012 at 05:46

Hi,

Thanks for replying.

But I am still having my confusion.

It is true that STM32L is a 32 bit micro controller.

But if I am having the following definition in my linker configuration file,

define block CSTACK    with alignment = 8, size = __ICFEDIT_size_cstack__   { };

alignment = 8 means, I am aligning my stack to 8 bytes.

Is that mean my stack width is 8 bytes?

Any clarifications regrading this will be highly appreciated.

Thank you.

frankmeyer9
Associate II
Posted on April 20, 2012 at 09:09

An alignment of 8 means that the stack begins at an address which is a multiple of 8. This is no architectural constraint, because most of the data handled with the stack are 32 bit.

This 8 byte alignment is a requirement for the ARM architecture ABI. It is assumed to make object files / libraries easily exchangable, i.e., you can link in a libraries compiled with a different toolchains.

Suggested reading: AppsNote179.pdf and IHI0046B_ABI_Advisory_1.pdf from

http://infocenter.arm.com

nanayakkaraan
Associate II
Posted on April 20, 2012 at 13:57

Hi fm,

Thanks for your reply and the given resource links.

I will go through it.

This means the stack width (stack word size) of STM32L is 4 bytes or 32 bit.

Thank you.

Posted on April 20, 2012 at 14:27

Unless you intentionally break the alignment playing with the SP, the push/pop will keep the alignment at 32-bits.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..