cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l151 not transmitting

bigblock14
Associate
Posted on January 21, 2014 at 04:13

Hi, this is my first post and first time working on an stm, so I am a bit new to this. I have a circuit I have been working on as a hobby. When the circuit is receiving, it is getting data from a device, and when it is transmitting, it is charging the device. Something is wrong, and the frustrating part is that it compiles correctly. I am looking for advice on things to look into or to think about. I feel that general discussion on this will help me. Thanks a ton.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
chen
Associate II
Posted on January 21, 2014 at 11:01

Hi

Welcome. Sorry but you have not given enough information for anybody to help you!

'' I have a circuit I have been working on as a hobby. When the circuit is receiving, it is getting data from a device, and when it is transmitting, it is charging the device.''

What is the circuit?

What is sending/recieving (USART, USB, I2C SPI)?

Charging - what are you charging?

''Something is wrong, and the frustrating part is that it compiles correctly.''

Just because he code compiles - does not mean that the circuit is correct.

Does not mean that the core if configured correctly.

Does not mean the peripherals are configured correctly.

Frustrated - So are we - give us a clue!