STM32L053C8Tx HAL UART DMA Bug at Overrun Error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-01-25 2:21 AM
Hi,
i found a bug in the HAL library for STM32L053C8Tx, when using UART with DMA. STMCube says its version STM32Cube FW_L0 V1.10.0
It seems that, in HAL_UART_IRQHandler the DMA should be reset when an Error occurs.
In a first step, the DMA request is disabled with CLEAR_BIT(huart->Instance->CR3, USART_CR3_DMAR); in line 1704 in stm32l0xx_har_uart.c
The program then jumps to HAL_DMA_Abort_IT at line 487 in stm32l0xx_hal_dma.c to reset the DMA.
It will only reset the DMA if hdma->State is HAL_DMA_STATE_BUSY. In my case, hdma->State is HAL_DMA_STATE_HALF_READY, which in my eyes qualifies as busy, but of course HAL_DMA_Abort_IT returns with HAL_ERROR, because its not HAL_DMA_STATE_BUSY. Thats why the DMA never gets reset, the Lock is still locked and state is still HAL_DMA_STATE_HALF_READY.
This results in very strange behaviour when using DMA after the error, as Rxcount, destination and source can't be changed. Calls to HAL_UART_DMAStop or HAL_UART_Abort won't do the trick, as USART_CR3_DMAR was cleared, making the program assume that DMA was properly reset.
I also use an STM32F0, which in my understanding has a slightly different HAL lib. In my STM32F0 project i couldn't find HAL_DMA_STATE_HALF_READY. It seems to me like that state was removed from some part of the HAL universe, but surely it was not done properly.
I hope this error gets fixed, either by eliminating HAL_DMA_STATE_HALF_READY or allowing HAL_DMA_Abort_IT to abort with state = HAL_DMA_STATE_HALF_READY.
Also i think it problematic to rely on USART_CR3_DMAR only to check if any DMA changes are needed, though there are many other variables that need to be changed to make the HAL lib work..
Maybe
LE_SAINT.Erwan
‌ or any member of the HAL development team can help here?Thanks,
Till
null- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-01-29 7:15 AM
Hello
till.rachow
,Thank you for your report issue. We will check this issue and inform you about the taken action.
Best Regards,
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-04 1:45 AM
Hi,
thanks! I just realized its HAL_DMA_STATE_READY_HALF instead of HAL_DMA_STATE_HALF_READY.
The problem still exists though, this was just a typo in my post.
Regards
Till