cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L temperature trimming values 90° or 110°

hartmann
Associate
Posted on October 10, 2012 at 09:25

Hello,

currently I'm evaluating the internal temperature senor of the STM32L151, but in the docs are different values for trimming values given. Sometimes 90° is stated somtimes 110°, so which value is correct?

STM32L151xx datasheet -> 110° for upper factory trimming value

STM32L151xx errata     ->    90°

RM0038 reference manual -> 90°

regards

thomas
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
raptorhal2
Lead
Posted on October 10, 2012 at 16:05

In fact it doesn't matter. The relevant advice from the user manual is:

To reduce the temperature sensor error, the user can measure it at ambient temperature

 

(25°C) to redefine more accurately the average slope (avg_slope) and the offset.

The temperature sensor has an offset that varies from one processor to another, so each processor needs to be calibrated.

If your design is for a production run, an external temperature sensor with less variation in offset might be more suitable.

Cheers, Hal

sheldon
Associate II
Posted on October 16, 2012 at 01:54

I just received an email from ST stating:

I have preliminary information from our factory, and it appears STM32Ls high density such as yours have correctly programmed engineering data only starting from revision Y (newer than your revision Z).

All previous revisions are susceptible to bad engineering data programming.

(I'm using STM32L152VC)

raptorhal2
Lead
Posted on October 16, 2012 at 15:28

Now we just have to figure out the algorithm difference between ''

correctly programmed engineering data

'' and

''bad engineering data programming''.

STOne - What is the design slope and offset for Revision Z ? Is there a way that Revision C can be used to measure internal temperature ?

If all else fails, with Rev C use actual readings with the processor in a plastic bag in ice water, then at room temperature, then in your expected usage environment with a thermometer nearby. For production, you should switch to Rev Z.

Cheers, Hal