cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L-Discovery communicate in I2C with M24LR64

Posted on April 24, 2012 at 09:13

Hello everybody,

I have some troubel to communicate with m24LR64. I use a STM32L- Discovery.

I try to see something in the oscilloscope but nothing, could you help me to see what is wrong in my code:

#define I2C2_SLAVE_ADDRESS7     0xA0   // EEPROM I2C Address

#define ClockSpeed              200000 // 200 KHz

#include ''mainsee.h''

void I2Cmain(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

I2C_InitTypeDef  I2C_InitStructure;

       

  /* I2C1 and I2C2 Periph clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE);

  /* GPIOB Periph clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

 

  /* Configure I2C2 pins: SCL and SDA ----------------------------------------*/

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_10 | GPIO_Pin_11;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOB, &GPIO_InitStructure);

  GPIO_PinAFConfig(GPIOB, GPIO_Pin_10, GPIO_AF_I2C2);

  GPIO_PinAFConfig(GPIOB, GPIO_Pin_11, GPIO_AF_I2C2);

  //I2C_DeInit(I2C2);    

           

  /* I2C2 configuration ------------------------------------------------------*/

  I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

  I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

  I2C_InitStructure.I2C_OwnAddress1 = I2C2_SLAVE_ADDRESS7;

  I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

  I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

  I2C_InitStructure.I2C_ClockSpeed = ClockSpeed;

  I2C_Init(I2C2, &I2C_InitStructure);

  /* Enable I2C2 -------------------------------------------------------------*/

  I2C_Cmd(I2C2, ENABLE);

  /* Send I2C1 START condition */

  I2C_GenerateSTART(I2C2, ENABLE);

  /* Test on I2C1 EV5 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT));

   /* Send EEPROM slave Address for write */

  //I2C_Send7bitAddress(I2C2, I2C2_SLAVE_ADDRESS7, I2C_Direction_Transmitter);  }

  /* Test on I2C1 EV6 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

 while(1){

  /* Send I2C1 EEPROM internal address */

  I2C_SendData(I2C2, 0x00);   }

  /* Test on I2C1 EV8 and clear it */

  while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

  /* Send I2C1 EEPROM data */

  I2C_SendData(I2C2, 0x05);

  /* Test on I2C1 EV8 and clear it */

  while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

  /* Send I2C1 STOP Condition */

  I2C_GenerateSTOP(I2C2, ENABLE);

  while(1); // Do not exit

}

Thank you very much in advance to help me.

P.S: Sorry for the english, i'm French.

20 REPLIES 20
Amel NASRI
ST Employee
Posted on January 07, 2015 at 09:31

Hello Siddharth,

This is an old thread. Please try to describe your problem in a separate discussion giving more details on your case. This will be easier to provide you help.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.