cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 i2c TC status not consistent with the reference documentation

JTse.1
Associate II

 

hi all

I have a weird operation on the I2C2 in STM32H743ZI cpu

i am sending 2 bytes to a I2c slave PCA9536DP, address= 0x41

the operation works and the slave IC did toggle the outputs BUT

at the end of the I2C2 transfer, the TC bit did not set even though the manual says it should.

is that normal?

see dump of the registers during the operation

OP: operation, CR1: contents of I2C2_CR1, ISR: contents of I2C2_ISR

   OP: CR1:     ISR:       comments 
   ISR:00020082 00000001 = condition before start of operation and start bit issued
   STR:00022082 00008001 = busy bit on after start bit issued
  Dta1:00020082 00008003 = first byte send and can send 2nd byte
  Dta2:00020082 00008000 = second byte send and tx reg not empty
  DtaE:00020082 00008001 = second byte send complete and tx reg empty
   STP:00000082 00000031 = stop bit send and detected, 
transmission completed; results appeared at the slave ic outputs
BUT TC is still not set and therefore not working at all, since all operation completed, it should have set
what is wrong??

 

1 REPLY 1
KDJEM.1
ST Employee

Hello @JTse.1,

 

I apologize for my late reply. 

Could you please try to reset the I2C peripheral after configuring the GPIOs like this: 

__HAL_RCC_I2C2_FORCE_RESET(); __HAL_RCC_I2C2_RELEASE_RESET();

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.